Electric power drives development and progress in all areas of everyday life. In Colombia, the partnership between WEG and CHEC S.A.E.S.P. BIC (a company of the EPM Group) will lead to a more reliable energy supply across the country.

The supply includes two three-phase 60 MVA transformers and two three-phase 40 MVA transformers, both of the 145 kV class. It also includes three single-phase 50 MVA autotransformers, 245 kV class, manufactured in the Gravataí and Blumenau plants in Brazil, in addition to one three-phase 4 MVA transformer, two three-phase 12.5 MVA transformers, two three-phase 20 MVA transformers, and one three-phase 300 kVA transformer manufactured in the Sabaneta’s plant in Colombia. The transformers belong to a three-year framework contract, reflecting the Latin American market's confidence in WEG's products and solutions.

These transformers will be installed in different substations in the CHEC market and will allow the expansion of the electrical system to ensure not only efficient energy distribution but also to strengthen the infrastructure to meet the growing demands of the Colombian population.

With this partnership, CHEC S.A.E.S.P. begins the path towards cleaner and more efficient energy, while WEG reinforces its contribution to a more reliable energy future.