Back to My Account
Consulte as dúvidas mais frequentes sobre o uso da solução WEG para produtos conectados.
The user can register the nameplate data manually through the field “I don't have a serial number”.
The WEG Motor Scan can be synchronized with the mobile app at approximately 10 meters or via gateway at approximately 30 meters. This is just a reference value, which may vary depending on the environment where the WEG Motor Scan and Gateway are installed.
No. The WEG Motor Scan application was developed to operate in environments without internet access. Measurements acquired by the smartphone or tablet during synchronization are stored and sent to the MFM software when the mobile device has internet access.
An event is characterized by the change in the state of one of the parameters that the WEG Motor Scan monitors. The change in the state indicates that one of the alarm criteria has been exceeded, both for the alert level and for the critical level.
When setting the alarm criteria levels, consider the application where the WEG Motor Scan is installed, and set appropriate values for the healthy operation of the motor, both for vibration and temperature, following the logic defined for the alarm criteria: Healthy (green): the motor is in its normal operating condition. Alert (yellow): scheduling a preventive stop of the motor is recommended for detailed diagnostics. Critical (red): an immediate corrective maintenance job on the motor is recommended.
Through the MFM software, on the asset screen, access the sensor data, click on "Tolerances". You can change the alert level and critical level values for vibration and temperature measurements.
Through the configuration options of the “Measurement unit” app.
The user can choose to collect data with the app using a smartphone or tablet; in this case, through a collection route or automatically through the WEG Motor Scan gateway (sold separately). The gateway connects to the sensor via Bluetooth and can send data to the WEG Motion Fleet Management software through a connection via Ethernet cable, Wi-Fi or 4G modem (via USB, not sold by WEG).
Our cloud partner is compliant and certified to standards ISO 27001; ISO 27017; ISO 27018; ISO 22301; ISO 31000; SOC 1, SOC 2 and SOC 3; PCI; HITRUST; ISO 9001; ISO 14001; ISO 50001 and OHSAS 1800; EU Model Clauses; FERPA; Cloud Computing Compliance Controls Catalog (C5) (Germany) and others. They provide a website that allows you to download various certifications. https://www.ibm.com/cloud/compliance. We use standard security protocols for user authentication (OpenID) and authorization (OAuth 2.0) for our website and mobile apps. WEG products are integrated with the WEG Motion Fleet Management software using the MQTT 3.1.1 protocol over the TLS 1.2+ protocol.
The WEG Motor Scan sensor can be synchronized with the gateway at approximately 30 meters. This is just a reference value, which may vary depending on the environment where the WEG Motor Scan and gateway are installed.
Up to 100 WEG Motor Scan sensors.
The WEG Motor Scan gateway can connect to the WEG Motion Fleet Management software via ethernet cable, Wi-Fi or 4G modem (via USB port). WEG does not sell the 4G modem. To obtain a 4G modem, contact your telephone company.
The gateway is powered over Ethernet (PoE) through its Ethernet port. If the user's network does not have this structure, or when the WI-FI or 4G modem connection is used, WEG provides a PoE injector power supply. See the instruction manual for installation.
Using the WEG Motor Scan app, choose the option "New Device", then click on "Select", gateway "Cassia X1000". Follow the guidelines presented in the app or refer to the instruction manual at https://static.weg.net/medias/downloadcenter/hfd/h51/WEG-motor-scan-gateway-cassia-X1000-manual-10008451731-en-en-es.pdf.
Yes. The sensor can be installed both in electric motors and in machines such as gearboxes, pumps, fans and compressors coupled to electric motors. In those kinds of machines, the WEG Motor Scan is registered as generic (other applications) and is intended for monitoring vibration and temperature. See the product manual to install the WEG Motor Scan on the machine.
The WEG Motor Scan application provides the instructions step-by-step. When asked about the asset type, select “Other” and proceed with the configuration. For more details, see the Sensor Configuration Manual at https://static.weg.net/medias/downloadcenter/h3e/h7c/WEG-motor-scan-mobile-app-manual-10008443991-pt-en-es.pdf.