WEG continues to offer its customers customized solutions for key applications where a provider with a complete product line and reliable performance is required. It's even better when the supply is part of the third project, previously involving two packages of WEG equipment that were sold and delivered.
The supply was carried out by Requip Cybersteel for the Manuelita Sugar Mill, located in Colombia. Requip Cybersteel is a strategic partner for WEG, delivering all equipment for the sugar mill and ensuring its commissioning with qualified personnel from the headquarters.
The scope of supply includes a medium voltage panel MTW03, 1250 A, a 24-pulse phase-shifting transformer, a medium voltage frequency drive MVW01 260 A, and a HGF motor, 1800 HP, 4160 V. These products will be used to drive the mills. The phase-shifting transformer, the medium voltage frequency drive, and the motor were manufactured at WEG in Brazil, while the medium voltage panel was produced at the Cota plant in Colombia.
The Manuelita Sugar Mill is a significant customer in Colombia's sugar sector, being one of the first mills and having made recurrent purchases of WEG equipment for mills, boilers, and energy generation and transmission.
The benefits provided to the client through this supply include improvements in the mill's indicators (sugar extraction and bagasse drying enhancement), which are critical parts of the process to increase sugar production, leading to greater efficiency and reduced downtime for equipment maintenance.
By choosing WEG solutions, the customer not only invests in advanced technology but also ensures the reliability and excellence of the project and installation.