WEG, official supplier of charging stations for electric vehicle brands, such as Peugeot, Fiat, Citroën, and Jeep in Brazil, expands its alliance with Stellantis to supply equipment for the group's affiliates in Argentina.

The agreement between the WEG branch and PEUGEOT in Argentina was reinforced with the launch of the new PEUGEOT 3008 HYBRID4 SUV, a 4x4 plug-in hybrid model, and provides the installation of WEMOB PARKING models at PEUGEOT dealerships in the country. Additionally, the agreement includes a WEMOB WALL model with each unit sold.

WEG charging station models deliver a modern, compact and easy-to-install design. The WALL model was specifically developed for internal and external use, with all the protections to be installed in a garage or home parking lot, with 7.4KW of power. The PARKING model with 22 KW of power, was created specifically for shared use in public and private parking lots, providing up to 3 times faster charging time.

WEG keeps focusing on the constant development of technology in order to serve this increasing market throughout the world, providing reliability and safety in all battery charging models.

ABOUT THE NEW PEUGEOT 3008 HYBRID4

The new PEUGEOT 3008 HYBRID4 SUV, a plug-in hybrid, delivers 300HP with its three engines, one combustion with 200HP and two electric 50HP each. It offers 4 driving modes, hybrid, electric, sport or 4x4, where the driver can choose depending on the terrain and the characteristics required at all times. By operating in 100% electric mode, it provides 58kms autonomy.