Phenom Parque Empresarial will be the first commercial development in the city of Maringá, Brazil, to offer an exclusive rooftop. With delivery scheduled for the end of 2025, the high-standard building will feature a unique space for events, meetings, and networking, with a spectacular view of the city, providing an unparalleled experience for its customers. The development is led by Marluc, a company with over 20 years of experience in the construction sector and a portfolio exceeding 1 million square meters built.
To ensure continuous and reliable operation, WEG, a leader in electrical equipment, will supply a set of essential products, including shielded busbars – Performance Line in aluminum with frames: 5000, 4000, 3200, 2500, and 800 A – totaling 675m, and transformers that together add up to more than 02 MVA of power. The shielded busbars are an alternative to electrical cables, offering savings and energy quality, while the transformers will be integrated into the substation of the enterprise, ensuring a safer and more efficient operation.
With these innovations, Phenom Parque Empresarial is positioned as a milestone in the architecture of the city of Maringá, exemplifying efficiency and modernity in the commercial sector, while the implementation of WEG's solutions will significantly contribute to the success of the project, aligning with the construction company's vision of creating a modern and functional space.
The combination of Marluc's expertise with WEG's technological solutions will provide valuable experiences to customers and strengthen the local economy by offering an environment conducive to networking and high-level events, establishing itself as one of the main business destinations in the region.