Ranked as one of the world's largest brands in the segment, Aquaturbo has again relied on WEG motor technology for a food industry wastewater treatment plant.
In this project, WEG Portugal supplied 10 motors W22 IE3 90 kW 6 poles which will drive the aerators at the station. The entire design was tailor-made for the Original Equipment Manufacturer and the green paint (RAL 6018) was added at the request of the End-User, a symbol of the energy efficiency that will be achieved with the use of WEG motors.
The W22 line stands out for promoting a reduction in energy consumption, offering an optimal cost-benefit balance and consequently greater productivity and reduced costs for the industry. Each kilowatt-hour that is saved in a production activity can be used to produce other products and services, and each monetary unit saved on energy is an additional resource for investments in innovation, productivity gains and compliance with sustainability goals.
WEG Portugal has a long-lasting partnership with Aquaturbo through our WEG Benelux branch and this supply reinforces the customer's confidence in WEG solutions.