返回到 我的账户
球磨机广泛应用于陶瓷和采矿业,其中研磨过程需要严格的粒度控制。
WEG为此应用开发了一种高效的解决方案,可将电能消耗降低最高达35%。 该解决方案由高效率产品组合而成:由CFW11变频器驱动W22 IR4永磁电机。可以调节电动机速度控制以便优化磨削过程,允许球之间的更大的接触从而使材料颗粒减小到期望的尺寸。
通过此种解决方案,增益超越了节能,还包括提高生产率,磨削周期更短,同样的磨机操作灵活性能够处理不同的材料并降低设备的机械磨损。
WEG and HORSE begin commercialization of the Range Extender
The partnership between the companies advances with the signing of the commercialization agreement, driving mobility
WEG 隆重推出 W51Xdb系列防爆电机
驱动一个更可持续的未来
WEG Transformers comprise the infrastructure of housing developments in Northern Brazil
The transformers will be present in the states of Tocantins and Pará
WEG Provides Solutions for Sugar and Ethanol Mills in Colombia
The equipment ensures a strong presence for the company in the sugar market
WEG supplies motors for a greenfield project on the cement sector in India
The complete package of motors will be manufactured at WEG’s facilities in Hosur
WEG is a Pioneer in Local Manufacturing of Medium Voltage Soft Starters in South Africa
The company has started producing medium voltage (MV) soft starters at one of its facilities in South Africa, reducing delivery times for customers and boosting local manufacturing
WEG supplies Motion Drives package to the tequila industry in Mexico
The integrated package ensures efficiency in the process, contributing to increased operational savings in the food and beverage industry
WEG replaces equipment and boosts energy efficiency in a French energy company
With this replacement, the customer ensured an increase of 15 to 18% in efficiency
WEG is taking part in the biggest power generation project using solid urban waste in Brazil
The project will not only help reduce environmental impact. It will also convert waste into clean energy that can supply power for approximately 320,000 people
WEG W30 Smart EC motors provide greater efficiency and sustainability at Granja Ueyama
Energy savings exceed 50%, in addition to advantages in dependability and greater animal comfort
WEGSEE+ is the definitive solution for optimizing resources in energy efficiency projects
Intuitive and complete software enables analysis of the impact caused by changes, even before they are made, reducing time and energy consumption and optimizing resources
WEG combina design moderno e melhor desempenho com nova linha de motores de chapa
W01 tem melhor relação peso potência para atender as demandas do mercado
WEG launches the most efficient industrial motor ever created, driving energy transition
Industry needs to keep growing, and the next steps are energy transition and avoiding carbon emissions
WEG-CESTARI provides a complete solution to enhance energy efficiency at Yara Brasil Fertilizers
WCG20 gearmotor line offers greater performance to the fertilizer industry
WEG supplies electric motors to the barrage of Kef Eddir-Tipaza in Algeria
The motors will be driven 14 lift stations