返回到 我的账户
用于驱动切碎机,整平机或粉碎机,无论配置如何,电机都采用最先进的工程设计,旨在实现高性能和高可靠性。 WEG电机的输出功率最高达50,000 kW,机座从280到1800(IEC标准),电机工作电压最高达13,800 V,它们提供两种转子配置:鼠笼和绕线转子(也称为绕线转子电机)。
WEG Provides Solutions for Sugar and Ethanol Mills in Colombia
The equipment ensures a strong presence for the company in the sugar market
WEG supplies Motion Drives package to the tequila industry in Mexico
The integrated package ensures efficiency in the process, contributing to increased operational savings in the food and beverage industry
WEG generator contributes to expansion of sugar and ethanol plant
The company provided a customized solution to meet the customer's needs
WEG supplies a tailor-made generator for the expansion of a corn ethanol plant in South America
The solution was designed to replace the existing equipment in order to increase the generation capacity and performance of the plant
WEG will be present at Fenasucro and Agrocana 2023
Fair takes place from August 15 to 18, at Centro de Eventos Zanini, in the city of Sertãozinho, São Paulo
WEG solutions equip two more sugar and ethanol plants in Brazil
The Slip Ring motors will ensure greater process reliability and less impact on the electrical system during equipment startup
WEG makes a new supply of mechanical drives for Usina Batatais
The solutions contribute to the modernization of mills, providing more productivity and efficiency to the operation
WEG participates in the expansion of the mill's crushing capacity
Equipment provided will trigger the sugarcane preparation process, chipper and shredder
WEG supplies one of the largest electric power generation equipment in Brazil for the sugar-energy industry sector
Cerradão power plant leverages its electricity generation with one of the largest equipment in the sector in Brazil.
WEG Planetary Gearboxes stands out in African Markets
Some units are successfully operating in sugars mills in Zimbabwe and Angola.
Turbine enables 13% gain in power generation
The new equipment uses the same amount of steam for additional generation of 3.0 MW / h
WEG solution will modernize sugar mill that operates with a maximum speed of 14 rpm
The replacement of traditional drives by this TGM solution will reduce maintenance costs, increase operational availability in addition to safety and greater ease during operation.
WEG equipment reduces and controls the final humidity in Vale do Paraná to 47%
Planetary gearbox, electric motor and drives are responsible for driving the 94” drying mill
WEG supplies electrical package to Alcooad's corn-based ethanol plant
Located in the state of Mato Grosso, Brazil, the plant will have the capacity to produce 225 million liters of ethanol per harvest.
WEG is the Technology Sponsor at IBC Sugar 2018 in Vietnam
The company will bring its knowledge and expertise presenting case studies about Power Consumption Improvement at the 24th Annual Asia International Sugar Conference 4–6 December 2018, Vietnam.
带着您的疑问联系我们